您需要什么帮助?
分类
PCB & PCBA
1. What files do I need to prepare to get a quotation for PCB & PCBA?
2. How can I get a quotation for PCB & PCBA?
3. How long it takes to get a quotation for PCB and PCBA?
4. What is the build time for PCB and PCBA?
5. What is the MOQ for PCB and PCBA?
6. What are the main products of your PCB & PCBA services?
7. How to get coupons for PCB and PCBA?
8. How to use the coupon for my order of PCB and PCBA?
9. How can I get support for PCB and PCBA?
10. How can you ensure the confidentiality of our PCB & PCBA files and information?
11. How to do the Solder-Resistance Bridges for printed circuit board?
12. What will you do with the English descriptions and other attachments in the zip file for the printed circuit board?
13. What if PCB file and Gerber file in the zip file at the same time?
14. How to do the Plated Edges or Slots for the printed circuit board?
15. Who is responsible for the issue with Software Incompatibility of the printed circuit board?
16. How do you deal with the markings on Base Materials?
17. What if my design has V-Cuts, Cutouts, Millings, and Slots for the printed circuit board?
18. Gerber View
19. What is the smallest text you can print on the boards during PCB assembly?
20. Can I place an order for 3-layer PCB fabrication?
21. How to place a repeat order correctly?
22. What are the design standards for the board outlines?
23. Can you produce printed circuit boards larger than 200mm x 250mm?
24. What should be considered regarding the thickness of the board outline, slots, cutouts, and milling?
25. What is your suggestions for boards within or less than 50mm x 50mm?
26. Could you tell me the maximum dimensions for assembling a PCB board? We have different sizes for various order types.
27. In a flex PCB design, which stiffener types do you support?
28. How long can a PCB board be effectively utilized?
29. What is the value of the FR-4 dielectric constant or relative permittivity for FR-4 used in the 1 oz, 2-layer PCB board?
30. Can you provide the temperature/fire class (for conformity with EN62368-1), the toxic substances (RoHS 3 statement), and the SVHC statement for my FR-4 board orders?
31. Can I know the layer stack values for aluminum base?
32. Can through-hole connectors be utilized in an aluminum PCB to link to the copper layer, or do they risk short-circuiting with the aluminum substrate?
33. What is the maximum temperature that could be used in the reflow oven for soldering flex PCBs?
34. Can you proceed without surface finishing on the PCB?
35. In a custom printed circuit board, what is the required file format for the drill file extension?
36. Our Project Involves Producing a 4-Layer Rigid PCB with a Thickness of 2mm and 2 Oz Copper Thickness on Both the Inner and Outer Layers. Is It Possible to Keep a Track Width and Clearance of 6 Mil?
37. Is It Required for Me to Mirror My PCB Design Before I Upload the Gerber Files, or Do You Take Care of This Automatically? It's a One-Sided PCB.
38. Given That We Can Only Employ Plated Through Holes (PTH) and Not Blind Vias on Four-Layer Circuit Boards, How Do We Achieve Interconnection Between the Mid Layers?
39. In a 2-Layer Flexible PCB, Is the Stiffener Located Between the Two Layers?
40. How Many Times Are Your Flexible PCBs Rated for Flexing? I Need to Choose a Flexible PCB for an Application Involving a Constantly Moving Carriage, and It’s Important to Ensure the Ratings Are Sufficient.
41. What documents are required for PCBA orders?
42. Do you support both SMD and THT components for PCB assembly?
43. Do you assemble boards with surface mount components on both sides?
44. Do you support downloading the corrected Pick and Place file for PCBA from your system?
45. What packages are supported by the economical PCB assembly service?
46. What does your quotation include for PCB assembly?
47. Do you support assembling THT components? What is the cost?
48. Do you accept components supplied by customers?
49. What are your requirements for the panelized board?
50. Do I need to add fiducial marks myself?
51. Do you offer assembly on boards fabricated by another company?
52. Do you support BGA component assembly?
What are the main products of your PCB & PCBA services?
Consumer electronics, industrial control, medical electronics, aerospace electronics, etc.